This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

mpeg2 with MP@ML stream



Hi

I have a problem related to the mpeg2. The elementary stream is MP@ML for HD, which is working wit the dvsdk_2_00_00_22 (cs2dm6467_1_00_00_10). As we need the H.264 update, I use the dvsdk_3_10_00_19 (cs2dm6467_1_00_00_10). It is not working with this stream anymore. I tried the CE_DEBUG=3 to see anything special in the DSP communication. I don't see any different. The attached file is the

 

2117.8055.Bug5342_Jul5_1.TXT (dvsdk_3_10_00_19 version)

5857.0045.Bug5342_sw134_Jul5_1.txt 

(dvsdk_2_00_00_22 version)

 elementary stream file.

1513.0647.test.zip 

Best Regards,

Philip Lee