This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x EVM baseboard PWRONRST & RTC_PWRONRST

Other Parts Discussed in Thread: AM3359, TPS65910

Hi

I'm working on a project based on an AM3359 with TPS65910AA1 power controller.

The EMV baseboard schematic manages the PORZ and RTC_PORZ signal with

two gate AND powered by VRTC. (1.8V)

The TPS65910  RESPWON signal ( 3.3V) feed the U1A gate (power 1.8V, 3.3V tollerant).

The U1A output feeds the AM335x PWRONRST input pin (power VDDSHV6 = VAUX2 = 3.3V).

Is this ok?

Thank you in advance

Regards

Andrea Sorio