This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

jpeg_encode lib



I want to ask the difference of the c64xplus_jpegenc_02_00_01_00_production and the dm648_jpegenc_1_12_001_production.

I development platform is DM648, could you tell me which library use encode performance higher.

I'm trying used the dm648_jpegenc_1_12_001_production

Code Generation :6.1.12

BIOS:5.41.03.17

CCS:3.3.82.10

I can bulid it but I can't run it,it can't pass the init.so whst should Ido?