This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RAM issue



Hello

I have planned to design android device with reference of AM335x EVM dev board OS is ANDROID ICS. i guess they are using two number of 256MB DDR2 RAM. Regarding this i need advice in following tasks

1. Can i use single piece of 1GB RAM instead of 512MB RAM.? if i use 1GB RAM it Will speed up my device or 512 & 1GB RAM have same speed.?

2. Can i use DDR3 RAM it will speed up my device.? if its speed my device do i have to add any additional hardware for DDR3 RAM..?

I need clear idea about DDR2 or DDR3.? and 1GB or 512MB RAM.?

Thanks in advance.

-- 

Regards

Sangilikumar M