Other Parts Discussed in Thread: TMS320C5535
Hello,
We are looking for a replacement to the TUSB3200CPAH and are investigating the suggested TMS320C5535. Our existing design has the TUSB3200CPAH configured as a single 7.1 interface. We are flexible on this so long that we keep the same number of channels. I've been digging through the Connected Audio Framework documentation and have not found anything indicating the configuration options of USB Audio Class.
Does anyone know first hand if the TMS3200C5535 along with the USB Audio Class Framework can support 8 channels USB in to 4 I2S Out? The processor comparison page:
Shows under USB Features -
TUSB3200A
Control Endpoint + 7 IN endpoints and 7 OUT endpoints
TNS320C5533
Control Endpoint + 4 IN endpoints and 4 OUT endpoints.
But I'm not sure how to interpret this.
What does 4 IN endpoints actually mean?
4 USB streams, or 4 channels in?
Our design needs to be able to receive a total of 8 channels over USB and output 8 digital channels (I2S). The hardware looks like it supports this but I want to be sure there isn't anything in the framework that would preclude me from doing that?
Thanks,
Andrew