The VPFE can act as master mode with the vertical and horizontal synchs being driven by the DM368. In the data sheet it claims that the pclk is an input only but later refers to different timings for the pclk in master mode. Can the DM368 drive the pclk in master mode? If not, what would be the ideal way to ensure proper data timing when taking in two streams of video through the front end?