Other Parts Discussed in Thread: OMAP-L138, DP83630
Hi Everyone,
We are using OMAP-L138 on a custom board where it interfaces to LAN8720A through RMII interface.
The PHY output passes through a simple header to connect to the RJ45 connector (with built in magnetics) on a separate board.
The distance between PHY and the RJ45 connector is around 2 inches.
Our setup uses a point-to-point connection between our board and the PC(server).
The problem:
When the UBoot downloads the UImage from the server over Ethernet in 100Mbps mode, we see that the download pauses several times before completion.
But, the download appears very smooth, without any pause, when the PHY has negotiated to 10Mbps mode.
We observe the same behaviour when using LAN8720 on the UI board connected to Zoom board.
On the contrary, the pauses seem to disappear when the connection to the server is through a network switch connected to our office LAN.
Has anyone faced a similar problem?
Kindly suggest.
Harshith