This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IPOD streaming issue on OMAP3730

Hi,

I have a problem with usb IPOD streaming on omap3730. I have configured the HID & Audio interfaces using libusb. I can able to send/receive the data from the hid. But am not able to stream the data from the IPOD using ISO endpoint.  Issue  with this are all most all the packets contain NULL the data,  but the some of the packet contain the data valid data.

I have tested using the DVSDK version. ti-dvsdk_dm3730-evm_4_02_00_06 & ti-dvsdk_dm3730-evm_4_03_00_00.

Using same sample code I can stream the data from IPOD using native ubunu 10.04 m/c.

I don't know whats problem?  Or the ISO endpoint is n't working in this kernel version?

can anyone help solving the problems.

Regards,

Shashi