Hi everyone,
I face a problem with debugging IFR .
I'm using CCS v5.1 and SYS/BIOS v6 .
here is the problem : I configured a GPIO (bank 7) pin (PIN 4) to signal event on rising edge (Event no 72) which in turn generates interrupt using HWI no 6 .
All that is fine and works, but when i try to trace IFR6 when interrupt happens ,IFR value is not updated although IER6 is enabled and ISR code is executed.
So, why IFR value doesn't change?