Other Parts Discussed in Thread: AM3517
Hi,
i have a problem with configuring LCD display on my AM3517,
UMSH-8253MD-T data sheet can be downloaded here -> http://firmware.avspekter.si/LCD%20Display.pdf
I did set
#if
defined(BSP_LCD_LB043WQ2)
{
/*OMAP_LCD_480W_272H*/
DISPC_PIXELFORMAT_RGB32, //pixelFmt;
480, //width;
272, //height;
41,//hsw;1 THP
2, //hfp2 je majka THB
2, //hbp;45 //2 ke dokaj lepo //10 je ful v desnpo zamakjen 1, sploh ne dela probam 70
10, //vsw;
2, //vfp;
2, //vbp;
1, //logClkDiv;
10, //pixelClkDiv;
(9 << 0),//dss1ClkSel;
0, //loadMode;
(DISPC_POL_FREQ_IVS | DISPC_POL_FREQ_IHS | DISPC_POL_FREQ_ONOFF),//polFreq;
0x00000000, //lcdDefaultColor;
0x00000000, //lcdTransColor;
0x00000000, //tvDefaultColor;
0x00000000, //tvTransColor;
},
What happens is that display is still moved to the right side, it is not fully alligned to left side, there are few pixels that are not used.
Can anyone help with this?
Best regards,
Luka