Hello,
I am doing RAM testing on the new board we just got with AM3359 chip on it. I can access OCMC RAM starting at 0x40300000 and load/execute code there, but I cannot read from and write to the internal RAM @ 0x402F0400 (question marks shown in the CCS). I am able to run the same code on the AM335x EVM (no OS loaded) with CCS 5.2. Is there anything I need to configure in order to see the internal RAM?
Please help.
Ying