This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Source level debug programs started by the on-chip boot loader?



Is source level debugging possible for programs started by the on-chip boot loader?

Using JTAG I can connect to the board, and download and run programs. I can write a program to flash that the on-chip boot loader will run out of reset without JTAG intervention. However I cannot source level debug that program.  I can stop and start it using pause/resume, and I can step through the disassembly.

From the debug configuration I set the loading options to load symbols only. I'm using CCSv5.2 with the C5504.