The AM3359 is powered by TPS65910AA1, the input voltage is 5V. When the power is supplied through a current meter, everything is OK, the board can work without problem. But with the current meter removed, AM3359 will burn out on power up. The VDDSHV(3.3V power path) pins will short to ground, AM3359 is totally damaged. I have double checked the input and output of TPS65910AA1, there is no problem found. I have tried 5 times, with current meter installed, everything is OK, removed, AM3359 burned instantly on power up. Does anyone have any troubleshooting tips for the problem? Any suggestion would be appreciated.