This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

rdk mcfw

 

root@dvr:~# ./gui.sh
*** Bootargs Validated for mem param ***
*** Bootargs Validated for notifyk.vpssm3 params ***
Kernel bootargs validated
numid=1,iface=MIXER,name='PCM Playback Volume'
  ; type=INTEGER,access=rw---R--,values=2,min=0,max=127,step=0
  : values=127,127
  | dBscale-min=-63.50dB,step=0.50dB,mute=0
SysLink version : 2.00.04.83
SysLink module created on Date:Mar  2 2012 Time:01:17:28
Trace enabled
Trace SetFailureReason enabled
 Setting DMM priority for [DUCATI  ] to [0] ( 0x4e000624 = 0x08000000 )
 Setting DMM priority for [HDVICP0 ] to [2] ( 0x4e000634 = 0x0000000a )
 Setting DMM priority for [HDVICP1 ] to [2] ( 0x4e000634 = 0x000a0000 )
 Setting DMM priority for [HDVICP2 ] to [2] ( 0x4e000634 = 0x00a00000 )
Attached to slave procId 2.
Loaded file ../firmware/dvr_rdk_fw_m3vpss.xem3 on slave procId 2.
Started slave procId 2.
After Ipc_loadcallback status [0x00000000]
After Ipc_startcallback status [0x097d2000]
Attached to slave procId 1.
Loaded file ../firmware/dvr_rdk_fw_m3video.xem3 on slave procId 1.
Started slave procId 1.
After Ipc_loadcallback status [0x00000000]
After Ipc_startcallback status [0x00000000]
Attached to slave procId 0.
Loaded file ../firmware/dvr_rdk_fw_c6xdsp.xe674 on slave procId 0.
Started slave procId 0.
After Ipc_loadcallback status [0x00000000]
After Ipc_startcallback status [0x00000000]
DMA: Module install successful, device major num = 251
DRV: Module install successful
DRV: Module built on Jun 26 2012 22:26:37
 [c6xdsp ] Remote Debug Shared Memory @ 0xbff00000
 [m3video] Remote Debug Shared Memory @ 0xbff05020
 [m3vpss ] Remote Debug Shared Memory @ 0xbff0a040
 [m3vpss ] Received character 's'
 [c6xdsp ] Remote Debug Shared Memory @ 0xbff00000
 [m3video] Remote Debug Shared Memory @ 0xbff05020
 [m3vpss ] Remote Debug Shared Memory @ 0xbff0a040
 [m3video] Received character 's'
 [c6xdsp ] Remote Debug Shared Memory @ 0xbff00000
 [m3video] Remote Debug Shared Memory @ 0xbff05020
 [m3vpss ] Remote Debug Shared Memory @ 0xbff0a040
 [c6xdsp ] Received character 's'
/opt/dvr_rdk/ti816x
VPSS_FVID2: M3 firmware version 0x1000136 is newer,driver may not work properly.
[module] vpss probe done.
[module] ti81xxfb probe done.
HDMI W1 rev 2.0
[module] ti81xx_hdmi probe done.
 
 ORG 0x46c00524: 0
 NEW 0x46c00524: 2
 
root@dvr:~# gVIDEOMOTION_ctrl.bufSize = 21120
gVIDEOMOTION_ctrl.bufNum  = 16
app_pb: app_playback_init ... success
--------------- CHANNEL DETAILS-------------
Capture Channels => 16
Enc Channels => Primary 16, Secondary 16
Dec Channels => 16
Disp Channels => 32
-------------------------------------------

 [host] APP_WRITER:SEND_streamFxn:Entered...
 [host] APP_WRITER:WRITER_videoRecvFxn:Entered...
 [host] APP_WRITER:WRITER_recordFxn:Entered... 0: SYSTEM: System Common Init in progress !!!
 0: SYSTEM: IPC init in progress !!!
 8: SYSTEM: Opening MsgQ Heap [IPC_MSGQ_MSG_HEAP] ...
 10: SYSTEM: Creating MsgQ [HOST_MSGQ] ...
 11: SYSTEM: Creating MsgQ [HOST_ACK_MSGQ] ...
 13: SYSTEM: Opening MsgQ [DSP_MSGQ] ...
 13: SYSTEM: Opening MsgQ [VIDEO-M3_MSGQ] ...
 14: SYSTEM: Opening MsgQ [VPSS-M3_MSGQ] ...
 14: SYSTEM: Notify register to [DSP] line 0, event 12 ...
 15: SYSTEM: Notify register to [VIDEO-M3] line 0, event 12 ...
 15: SYSTEM: Notify register to [VPSS-M3] line 0, event 12 ...
 16: SYSTEM: IPC init DONE !!!
 17: SYSTEM: Creating ListMP [HOST_IPC_OUT_29] in region 0 ...
 19: SYSTEM: Creating ListMP [HOST_IPC_IN_29] in region 0 ...
 20: SYSTEM: hrtimer: interrupt took 17704 ns
ListElem Shared Addr = 0x4c2da080
 21: SYSTEM: Creating ListMP [HOST_IPC_OUT_30] in region 0 ...
 23: SYSTEM: Creating ListMP [HOST_IPC_IN_30] in region 0 ...
 24: SYSTEM: ListElem Shared Addr = 0x4c2f1980
IpcBitsOutlink----------ok
IpcFramesInLink----------ok
 26: SYSTEM: Creating ListMP [HOST_IPC_OUT_24] in region 0 ...
 28: SYSTEM: Creating ListMP [HOST_IPC_IN_24] in region 0 ...
 29: SYSTEM: ListElem Shared Addr = 0x4c309280
 30: SYSTEM: Creating ListMP [HOST_IPC_OUT_25] in region 0 ...
 32: SYSTEM: Creating ListMP [HOST_IPC_IN_25] in region 0 ...
 34: SYSTEM: ListElem Shared Addr = 0x4c328880
 35: SYSTEM: Creating ListMP [HOST_IPC_OUT_26] in region 0 ...
 37: SYSTEM: Creating ListMP [HOST_IPC_IN_26] in region 0 ...
 38: SYSTEM: ListElem Shared Addr = 0x4c347e80
IpcFramesOutLink----------ok
 39: SYSTEM: System Common Init Done !!!
AVSYNC_Init start


=============== AVSYNC_curTime = 1336521640404 ==================
AVSYNC_Init done

********* Entered usecase 16CH Progressive <816x> Cap/Enc/Dec/Dis

 40: MCFW  : CPU Revision [ES1.1] !!!
 40: MCFW  : Detected [(null)] Board !!!
 40: MCFW  : Base Board Revision [DVR] !!!
 40: MCFW  : Daughter Card Revision [DVR] !!!
111
222
333
44444
55555
6666
6666--0000
6666-----1111
6666-----2222
7777

 [host] IpcBitsInLink_tskMain:Entered
 [host]  7919: IPC_BITS_IN   : Create in progress !!!

 [host]  7919: IPC_BITS_IN   : ListMPOpen start !!!

 [host]  7919: SYSTEM: Opening ListMP [VIDEO-M3_IPC_OUT_29] ...
 7921: SYSTEM: Opening ListMP [VIDEO-M3_IPC_IN_29] ...

 [host]  7922: IPC_BITS_IN   : ListMPOpen done !!!

 [host]  7924: IPC_BITS_IN   : System_linkGetInfo done !!!

 [host]  7924: IPC_BITS_IN   : Create Done !!!
8888
Reducing bitsProducerLinkInfo.numCh to 16
mul:0,1280,720
mul:1,1280,720
mul:2,1280,720
mul:3,1280,720
mul:4,1280,720
mul:5,1280,720
mul:6,1280,720
mul:7,1280,720
mul:8,1280,720
mul:9,1280,720
mul:10,1280,720
mul:11,1280,720
mul:12,1280,720
mul:13,1280,720
mul:14,1280,720
mul:15,1280,720
bitout-------11111

 [host]  7924: IPC_BITS_OUT   : Create in progress !!!
 ASSERT (ipcBitsOutLink_tsk.c|IpcBitsOutLink_createOutObj|383)

 

when I run the "vcap_venc_vdec_vdis" demo,it stop here.why?