This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Format SATA Fails



I'm trying to format my 2TB HDD connected to SATA0 on the EVM. I am able to see /dev/sda and so i created a partition using fdisk. When I try to format using mfks, mkfs.ext2, mke2fs, ect. it starts the process and then epic fails. Here is my console output:

root@dm816x-evm:~# fdisk /dev/sda                                               
                                                                                
The number of cylinders for this disk is set to 243201.                         
There is nothing wrong with that, but this is larger than 1024,                 
and could in certain setups cause problems with:                                
1) software that runs at boot time (e.g., old versions of LILO)                 
2) booting and partitioning software from other OSs                             
   (e.g., DOS FDISK, OS/2 FDISK)                                                
                                                                                
Command (m for help): n                                                         
Command action                                                                  
   e   extended                                                                 
   p   primary partition (1-4)                                                  
p                                                                               
Partition number (1-4): 1                                                       
First cylinder (1-243201, default 1):                                           
Using default value 1                                                           
Last cylinder, +cylinders or +size{K,M,G} (1-243201, default 243201):           
Using default value 243201                                                      
                                                                                
Command (m for help): p                                                         
                                                                                
Disk /dev/sda: 2000.4 GB, 2000398934016 bytes                                   
255 heads, 63 sectors/track, 243201 cylinders                                   
Units = cylinders of 16065 * 512 = 8225280 bytes                                
Sector size (logical/physical): 512 bytes / 512 bytes                           
Disk identifier: 0xff4e0f0b                                                     
                                                                                
   Device Boot      Start         End      Blocks   Id  System                  
/dev/sda1               1      243201  1953512001   83  Linux                   
                                                                                
Command (m for help): t                                                         
Selected partition 1                                                            
Hex code (type L to list codes): 83                                             
                                                                                
Command (m for help): w                                                         
The partition table has been altered!                                           
                                                                                
Calling sda: sda1                                                               
 ioctl() to re-read partition table.                                            
Syncing disks.                                                                  
root@dm816x-evm:~# FAT: bogus number of reserved sectors                        
VFS: Can't find a valid FAT filesystem on dev sda1.                             
                                                                                
root@dm816x-evm:~# mkfs -t ext2 /dev/sda1                                       
mke2fs 1.41.14 (22-Dec-2010)                                                    
Filesystem label=                                                               
OS type: Linux                                                                  
Block size=4096 (log=2)                                                         
Fragment size=4096 (log=2)                                                      
Stride=0 blocks, Stripe width=0 blocks                                          
122101760 inodes, 488378000 blocks                                              
24418900 blocks (5.00%) reserved for the super user                             
First data block=0                                                              
Maximum filesystem blocks=0                                                     
14905 block groups                                                              
32768 blocks per group, 32768 fragments per group                               
8192 inodes per group                                                           
Superblock backups stored on blocks:                                            
        32768, 98304, 163840, 229376, 294912, 819200, 884736, 1605632, 2654208,
        4096000, 7962624, 11239424, 20480000, 23887872, 71663616, 78675968,     
        102400000, 214990848                                                    
                                                                                
Writing inode tables: Unable to handle kernel paging request at virtual address
70050000                                                                        
pgd = c0004000                                                                  
[70050000] *pgd=00000000                                                        
Internal error: Oops: 805 [#1]                                                  
last sysfs file: /sys/devices/platform/ahci.0/host0/target0:0:0/0:0:0:0/block/sd
a/removable                                                                     
Modules linked in: bufferclass_ti omaplfb pvrsrvkm ti81xxhdmi ti81xxfb vpss sysl
ink ipv6                                                                        
CPU: 0    Not tainted  (2.6.37 #1)                                              
PC is at move_freepages_block+0xd8/0x130                                        
LR is at __rmqueue+0x1e8/0x324                                                  
pc : [<c00a33f0>]    lr : [<c00a3694>]    psr: 00000093                         
sp : eeee5a70  ip : 00042302  fp : eeee5a94                                     
r10: 00000000  r9 : c051f4ec  r8 : c051f4ec                                     
r7 : c0952fe0  r6 : 00000004  r5 : c094b080  r4 : 78cf0f00                      
r3 : 00b60458  r2 : 00100100  r1 : 00000000  r0 : 70050000                      
Flags: nzcv  IRQs off  FIQs on  Mode SVC_32  ISA ARM  Segment kernel            
Control: 10c5387d  Table: aefcc019  DAC: 00000017                               
Process flush-8:0 (pid: 1463, stack limit = 0xeeee42e8)                         
Stack: (0xeeee5a70 to 0xeeee6000)                                               
5a60:                                     c094f000 00000009 c094f018 00000000   
5a80: 00000002 c051f69c eeee5acc eeee5a98 c00a3694 c00a3324 c00c2d94 00000000   
5aa0: ef801460 c0576ff8 0000000f c0bdf09c 60000093 00000000 c051f4ec c051f74c   
5ac0: eeee5b34 eeee5ad0 c00a4d64 c00a34b8 00000041 00011200 00000000 00031200   
5ae0: c051fdb0 00000000 00000000 ffffffff 00000001 0000001f 00000069 c0bdf0a8   
5b00: c01b70b0 c051f4ec 00000000 00011200 003fffff 00011200 ef802200 ffffffff   
5b20: eeee5ed0 00000000 eeee5bb4 eeee5b38 c00a516c c00a4c78 00000000 00000041   
5b40: c051f4ec 00000000 00000000 c051fda4 00031200 00000000 00000000 c051fda8   
5b60: 00080000 000828ab 00000000 00000000 00000001 00000001 eeee5b9c c0df0f80   
5b80: 00000000 c051f4ec eeee4000 ef801080 00011200 00000020 ef802200 ffffffff   
5ba0: eeee5ed0 c00a1600 eeee5bdc eeee5bb8 c00c2c0c c00a5080 ef801080 00000000   
5bc0: ef802200 00011200 ffffffff eeee5ed0 eeee5c04 eeee5be0 c00c2f14 c00c2bbc   
5be0: 00000000 40000013 ef802200 00011200 eeee4000 ef88af18 eeee5c2c eeee5c08   
5c00: c00c33b0 c00c2dd4 c0bdf030 00000002 00000001 c6b73690 ef88af00 00011210   
5c20: eeee5c3c eeee5c30 c00a1600 c00c3370 eeee5c7c eeee5c40 c00a17d0 c00a15f0   
5c40: 00000000 00000000 c6b73540 c0df0f80 00000000 c6b735e8 00000001 c6b73690   
5c60: 00000010 c6b736c8 ef88ae80 eeee5ed0 eeee5cac eeee5c80 c00ec0e0 c00a17a0   
5c80: 00000bb8 0000000f eeee5cb4 c6b736c8 c6b73690 00000001 c6b736c8 ef6ddaf0   
5ca0: eeee5cbc eeee5cb0 c00ec1e8 c00ec0bc eeee5cdc eeee5cc0 c00e775c c00ec1dc   
5cc0: 00000001 c6b73690 c05ac580 c6b736c8 eeee5d1c eeee5ce0 c00ea69c c00e76a0   
5ce0: c00ecf44 74703a40 00000400 00000001 c01b6444 ef6ddb94 eeee5ed0 ef6ddaf0   
5d00: c05ac580 c00ecf44 c00e9d30 eeee5ed0 eeee5d54 eeee5d20 c00ea8c4 c00ea3f0   
5d20: c00e9d30 eeee5d30 c009f0dc ef6ddb94 eeee5ed0 00000000 ffffffff 00000007   
5d40: 00000000 eeee5dd8 eeee5d64 eeee5d58 c00ea8e0 c00ea820 eeee5d74 eeee5d68   
5d60: c00ee0c8 c00ea8d8 eeee5d8c eeee5d78 c00a56f4 c00ee0bc c05ac580 eeee5ed0   
5d80: eeee5e2c eeee5d90 c00a606c c00a56e4 0000000e eeee5da0 ef6ddb94 c00a56d8   
5da0: ef6ddb94 0000000e 00598201 005a80fd 00000000 00000000 ffffffff 0000000e   
5dc0: 00000000 c05ac4a0 c05ac4c0 c05ac4e0 c05ac500 c05ac520 c05ac540 c05ac560   
5de0: c05ac580 c05ac5a0 c05ac5c0 c05ac5e0 c05ac600 c05ac620 c05ac640 005a8103   
5e00: eeee5ed0 ef6ddaf0 ef6ddaf0 eeee5ed0 ef6ddb94 00000000 efb73178 efb73180   
5e20: eeee5e3c eeee5e30 c00a617c c00a5e60 eeee5e4c eeee5e40 c00a61b8 c00a6158   
5e40: eeee5e6c eeee5e50 c00e1d2c c00a6190 00000000 ef6ddaf0 eeee5ed0 efb73140   
5e60: eeee5ea4 eeee5e70 c00e21ec c00e1c88 eeee5e70 ef803800 c00c80ec ef803840   
5e80: ef803800 efb73140 eeee5ed0 ef6ddaf0 00000000 efb73178 eeee5ecc eeee5ea8   
5ea0: c00e2798 c00e2158 00000000 00016800 efb73180 efb73178 efb73140 eefc3ac0   
5ec0: eeee5f34 eeee5ed0 c00e2944 c00e26c8 00000000 00000000 ffffbe84 00000105   
5ee0: 00000000 00000000 00000000 00000000 00000000 00000000 00000028 00000000   
5f00: c039f90c 00006184 000030c2 ef275b80 efb730e8 eefc3ac0 eeee4000 efb73140   
5f20: 00000000 efb73188 eeee5f84 eeee5f38 c00e2a04 c00e27c0 eeee5f5c eeee5f48   
5f40: c039f994 c039f95c 00000000 ef275b80 eeee5f84 efb73154 eeee5f84 efb73140   
5f60: 00000000 eeee4000 efb730e8 efb73188 efb73178 efb73180 eeee5fbc eeee5f88   
5f80: c00e2ba4 c00e29c0 efb73154 efb73170 c039c094 eeee5fcc ef89bef8 efb73140   
5fa0: c00e2b24 00000000 00000000 00000000 eeee5ff4 eeee5fc0 c00848c8 c00e2b30   
5fc0: ef89bef8 00000000 efb73140 00000000 eeee5fd0 eeee5fd0 ef89bef8 c008483c   
5fe0: c0070c28 00000013 00000000 eeee5ff8 c0070c28 c0084848 ffffffff ffffffff   
Backtrace:                                                                      
[<c00a3318>] (move_freepages_block+0x0/0x130) from [<c00a3694>] (__rmqueue+0x1e8
/0x324)                                                                         
[<c00a34ac>] (__rmqueue+0x0/0x324) from [<c00a4d64>] (get_page_from_freelist+0xf
8/0x408)                                                                        
[<c00a4c6c>] (get_page_from_freelist+0x0/0x408) from [<c00a516c>] (__alloc_pages
_nodemask+0xf8/0x51c)                                                           
[<c00a5074>] (__alloc_pages_nodemask+0x0/0x51c) from [<c00c2c0c>] (new_slab+0x5c
/0x218)                                                                         
[<c00c2bb0>] (new_slab+0x0/0x218) from [<c00c2f14>] (__slab_alloc+0x14c/0x228)  
 r9:eeee5ed0 r8:ffffffff r7:00011200 r6:ef802200 r5:00000000                    
r4:ef801080                                                                     
[<c00c2dc8>] (__slab_alloc+0x0/0x228) from [<c00c33b0>] (kmem_cache_alloc+0x4c/0
x84)                                                                            
[<c00c3364>] (kmem_cache_alloc+0x0/0x84) from [<c00a1600>] (mempool_alloc_slab+0
x1c/0x20)                                                                       
 r7:00011210 r6:ef88af00 r5:c6b73690 r4:00000001                                
[<c00a15e4>] (mempool_alloc_slab+0x0/0x20) from [<c00a17d0>] (mempool_alloc+0x3c
/0xe4)                                                                          
[<c00a1794>] (mempool_alloc+0x0/0xe4) from [<c00ec0e0>] (bio_alloc_bioset+0x30/0
xd4)                                                                            
[<c00ec0b0>] (bio_alloc_bioset+0x0/0xd4) from [<c00ec1e8>] (bio_alloc+0x18/0x30)
 r8:ef6ddaf0 r7:c6b736c8 r6:00000001 r5:c6b73690 r4:c6b736c8                    
[<c00ec1d0>] (bio_alloc+0x0/0x30) from [<c00e775c>] (submit_bh+0xc8/0x180)      
[<c00e7694>] (submit_bh+0x0/0x180) from [<c00ea69c>] (__block_write_full_page+0x
2b8/0x430)                                                                      
 r7:c6b736c8 r6:c05ac580 r5:c6b73690 r4:00000001                                
[<c00ea3e4>] (__block_write_full_page+0x0/0x430) from [<c00ea8c4>] (block_write_
full_page_endio+0xb0/0xb8)                                                      
[<c00ea814>] (block_write_full_page_endio+0x0/0xb8) from [<c00ea8e0>] (block_wri
te_full_page+0x14/0x1c)                                                         
[<c00ea8cc>] (block_write_full_page+0x0/0x1c) from [<c00ee0c8>] (blkdev_writepag
e+0x18/0x20)                                                                    
[<c00ee0b0>] (blkdev_writepage+0x0/0x20) from [<c00a56f4>] (__writepage+0x1c/0x6
4)                                                                              
[<c00a56d8>] (__writepage+0x0/0x64) from [<c00a606c>] (write_cache_pages+0x218/0
x2f8)                                                                           
 r5:eeee5ed0 r4:c05ac580                                                        
[<c00a5e54>] (write_cache_pages+0x0/0x2f8) from [<c00a617c>] (generic_writepages
+0x30/0x38)                                                                     
[<c00a614c>] (generic_writepages+0x0/0x38) from [<c00a61b8>] (do_writepages+0x34
/0x40)                                                                          
[<c00a6184>] (do_writepages+0x0/0x40) from [<c00e1d2c>] (writeback_single_inode+
0xb0/0x1c0)                                                                     
[<c00e1c7c>] (writeback_single_inode+0x0/0x1c0) from [<c00e21ec>] (writeback_sb_
inodes+0xa0/0x108)                                                              
 r7:efb73140 r6:eeee5ed0 r5:ef6ddaf0 r4:00000000                                
[<c00e214c>] (writeback_sb_inodes+0x0/0x108) from [<c00e2798>] (writeback_inodes
_wb+0xdc/0xf8)                                                                  
[<c00e26bc>] (writeback_inodes_wb+0x0/0xf8) from [<c00e2944>] (wb_writeback+0x19
0/0x200)                                                                        
[<c00e27b4>] (wb_writeback+0x0/0x200) from [<c00e2a04>] (wb_do_writeback+0x50/0x
170)                                                                            
[<c00e29b4>] (wb_do_writeback+0x0/0x170) from [<c00e2ba4>] (bdi_writeback_thread
+0x80/0x14c)                                                                    
[<c00e2b24>] (bdi_writeback_thread+0x0/0x14c) from [<c00848c8>] (kthread+0x8c/0x
94)                                                                             
[<c008483c>] (kthread+0x0/0x94) from [<c0070c28>] (do_exit+0x0/0x5e4)           
 r7:00000013 r6:c0070c28 r5:c008483c r4:ef89bef8                                
Code: e595001c e0866c12 e0030c93 e59f2050 (e5804000)                            
---[ end trace 0ef4431aaeb42bae ]---                                            
Unable to handle kernel paging request at virtual address 70050000              
pgd = eefcc000                                                                  
[70050000] *pgd=00000000                                                        
Internal error: Oops: 805 [#2]                                                  
last sysfs file: /sys/devices/platform/ahci.0/host0/target0:0:0/0:0:0:0/block/sd
a/removable                                                                     
Modules linked in: bufferclass_ti omaplfb pvrsrvkm ti81xxhdmi ti81xxfb vpss sysl
ink ipv6                                                                        
CPU: 0    Tainted: G      D      (2.6.37 #1)                                    
PC is at move_freepages_block+0xd8/0x130                                        
LR is at __rmqueue+0x1e8/0x324                                                  
pc : [<c00a33f0>]    lr : [<c00a3694>]    psr: 00000093                         
sp : ec867bd0  ip : 00042302  fp : ec867bf4                                     
r10: 00000000  r9 : c051f4ec  r8 : c051f4ec                                     
r7 : c0952fe0  r6 : 00000004  r5 : c094b080  r4 : 78cf0f00                      
r3 : 00b60458  r2 : 00100100  r1 : 00000000  r0 : 70050000                      
Flags: nzcv  IRQs off  FIQs on  Mode SVC_32  ISA ARM  Segment user              
Control: 10c5387d  Table: aefcc019  DAC: 00000015                               
Process mkfs.ext2 (pid: 1503, stack limit = 0xec8662e8)                         
Stack: (0xec867bd0 to 0xec868000)                                               
7bc0:                                     c094f000 00000009 c094f018 00000000   
7be0: 00000002 c051f69c ec867c2c ec867bf8 c00a3694 c00a3324 c00c2d94 00000000   
7c00: ef8012a0 c0576ff8 00000016 c0bdf09c 60000013 00000000 c051f4ec c051f74c   
7c20: ec867c94 ec867c30 c00a4d64 c00a34b8 00000041 00008050 00000000 000200d0   
7c40: c051fdb0 00000000 00000000 ffffffff 00000001 0000001f 00000047 c0bdf0a8   
7c60: e3b95118 c051f4ec eeee22a0 000200d0 003fffff 000200d0 ef6ddb94 0069002d   
7c80: ef6ddb94 00000000 ec867d14 ec867c98 c00a516c c00a4c78 00000000 00000041   
7ca0: c051f4ec 00000000 00000000 c051fda4 000200d0 00000000 00000000 c051fda8   
7cc0: c01b5bd8 c01b5b24 ec867cf4 ec867cd8 c009f3c8 c01b5bd0 00001000 ef6ddb94   
7ce0: 0069002d c051f4ec ec867d14 ffffffff 9002d000 00000000 ef6ddb94 0069002d   
7d00: ef6ddb94 00000000 ec867d3c ec867d18 c009fb18 c00a5080 00001000 9002d000   
7d20: 00000006 00000006 00001000 ec866000 ec867d64 ec867d40 c00e973c c009facc   
7d40: c009f718 c0084c8c c0b1f0c0 00001000 00005000 9002d000 ec867d84 ec867d68   
7d60: c00ee084 c00e9720 00001000 00000000 ec867dc4 c00ecf44 ec867df4 ec867d88   
7d80: c009ec50 c00ee058 00001000 00000000 ec867dc4 ec867dc0 c0072054 ef269b00   
7da0: 00001000 00000000 00000000 c03ab334 ec867f20 00000001 00005000 00003000   
7dc0: c00d88e8 c0b1f0c0 4f9dc611 90030000 00000006 00008000 ec867f20 90028000   
7de0: 00000006 00008000 ec867e6c ec867df8 c00a0a68 c009eb78 90028000 00000006   
7e00: ec867ee0 00008000 00000000 00000000 ec867ee0 ec867ea8 ef269b00 ef6ddb94   
7e20: 00000000 00000001 ef025000 ef909000 ef13bcc0 00000004 0000000a 00008000   
7e40: ec867e6c 00000006 90028000 ec867ea8 ef269b00 ef269b00 ec866000 00000000   
7e60: ec867e9c ec867e70 c00ed588 c00a064c 00008000 00000000 00000010 90028000   
7e80: 00000006 ec867ea8 ef269b00 ec867f70 ec867f4c ec867ea0 c00c6244 c00ed550   
7ea0: 90028000 00000006 ec867ec4 ec867eb8 00000000 00000001 ffffffff ef269b00   
7ec0: 00000000 00000000 00000000 00000000 eeee2000 ec867ee0 00000000 00000000   
7ee0: 90028000 00000006 c003b080 c0072c40 00008000 fa200000 00008000 ec867f08   
7f00: c019d644 c019db28 ec867f4c ec867f18 c00c644c c019d634 c00ed4f0 c039c728   
7f20: 00028278 00008000 ef269b00 ef269b00 00028278 ec867f70 00008000 00028278   
7f40: ec867f6c ec867f50 c00c6c3c c00c61b0 90028000 00000006 ef269b00 00008000   
7f60: ec867fa4 ec867f70 c00c6d28 c00c6b98 90028000 00000006 ec867fac 00000000   
7f80: c039c094 1a437000 00000000 00028278 00000004 c0045fa8 00000000 ec867fa8   
7fa0: c0045e00 c00c6cf0 1a437000 00000000 00000003 00028278 00008000 00000000   
7fc0: 1a437000 00000000 00028278 00000004 90028000 00000006 0001ec70 00008000   
7fe0: 0001ec08 bea3b858 400d1728 401ddabc 60000010 00000003 76c66e63 72d53c20   
Backtrace:                                                                      
[<c00a3318>] (move_freepages_block+0x0/0x130) from [<c00a3694>] (__rmqueue+0x1e8
/0x324)                                                                         
[<c00a34ac>] (__rmqueue+0x0/0x324) from [<c00a4d64>] (get_page_from_freelist+0xf
8/0x408)                                                                        
[<c00a4c6c>] (get_page_from_freelist+0x0/0x408) from [<c00a516c>] (__alloc_pages
_nodemask+0xf8/0x51c)                                                           
[<c00a5074>] (__alloc_pages_nodemask+0x0/0x51c) from [<c009fb18>] (grab_cache_pa
ge_write_begin+0x58/0x98)                                                       
[<c009fac0>] (grab_cache_page_write_begin+0x0/0x98) from [<c00e973c>] (block_wri
te_begin+0x28/0x80)                                                             
[<c00e9714>] (block_write_begin+0x0/0x80) from [<c00ee084>] (blkdev_write_begin+
0x38/0x44)                                                                      
 r6:9002d000 r5:00005000 r4:00001000                                            
[<c00ee04c>] (blkdev_write_begin+0x0/0x44) from [<c009ec50>] (generic_file_buffe
red_write+0xe4/0x21c)                                                           
[<c009eb6c>] (generic_file_buffered_write+0x0/0x21c) from [<c00a0a68>] (__generi
c_file_aio_write+0x428/0x478)                                                   
[<c00a0640>] (__generic_file_aio_write+0x0/0x478) from [<c00ed588>] (blkdev_aio_
write+0x44/0xa0)                                                                
[<c00ed544>] (blkdev_aio_write+0x0/0xa0) from [<c00c6244>] (do_sync_write+0xa0/0
xec)                                                                            
 r8:ec867f70 r7:ef269b00 r6:ec867ea8 r5:00000006 r4:90028000                    
[<c00c61a4>] (do_sync_write+0x0/0xec) from [<c00c6c3c>] (vfs_write+0xb0/0xd8)   
 r8:00028278 r7:00008000 r6:ec867f70 r5:00028278 r4:ef269b00                    
[<c00c6b8c>] (vfs_write+0x0/0xd8) from [<c00c6d28>] (sys_write+0x44/0x70)       
 r7:00008000 r6:ef269b00 r5:00000006 r4:90028000                                
[<c00c6ce4>] (sys_write+0x0/0x70) from [<c0045e00>] (ret_fast_syscall+0x0/0x30)
 r8:c0045fa8 r7:00000004 r6:00028278 r5:00000000 r4:1a437000                    
Code: e595001c e0866c12 e0030c93 e59f2050 (e5804000)                            
---[ end trace 0ef4431aaeb42baf ]---

What am I missing? Is the 2TB HDD just to much for the EVM? Is this because I'm booted NFS/TFTP?

Thanks All!

  • Hello, Troy Wood

    I tried to connect a SATA HDD to my dm816x. The format was successful, and I am coping files back and forth; it works. There are many possibilities what could be wrong on your side. You can try first with something more simple:

    <DM816X># mkdosfs -F32 -I /dev/sdX

    just to see is this working. Of cource you can always ext format the disk on your host and then attach it to the board. If you're still having problems, write again please.

    BR

  • I tried FAT32 as you suggested with similar errors and a failed result.

    I gave up and replaced the 2TB drive with a 1TB drive and the format at ext3 worked flawlessly. I am now capturing and playing back without fail.

    So it begs the questions, was the 2TB simply to much or was it a compatibility issue with the drive itself? It is 3Gbps so it should have worked, but I'll have to scratch it off the list of possible drives for the end product.

    Is there a list of tested HDD's in the 2TB flavor?

    Thanks-

  • Hello, Troy Wood

    I am not sure that such list (of tested HDDs) exists, I have to check this out, but I don't think that it should differs from a common Linux system. Currently I don't have a 2TB HDD, and I don't know that I'll be able to reproduce your issue, but I will try.

    Please tell me, what happens when you format the 2TB HDD on your Linux host and then connect it to the board, is it working that way?

    BR

  • Formatting on the host at ext3 and then connecting to the EVM works, not sure why formatting the same drive on the EVM would fail.

    I've ordered a 2TB drive from a different manufacturer to see if the problem persists, if not then I will just assume it is an incompatibility with that drive model.

    Thanks for your assistance-

    Troy

  • Hello, Try Wood

    Please inform me again when you test your new drive from different manufacturer; what was the behaviour. Thank you.

    BR