This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Build time optimization

Hi,

In the 3.0 release, whenever I try to do incremental builds such as “make mcfw_linux”, it does not populate the binaries created in the filesystem directory specified in Rules.make.  It only does so when I do a “make sysall”.  Earlier versions did not seem to have this issue.  Because of this I end up doing a full build for any small change in the code to make sure all binaries are getting pushed to appropriate directories.  Is there a way to do incremental builds and then also follow it up with making sure binaries are being pushed to the filesystem?

thanks,

Chandar