This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to integrate a static library to a DMAI application



I want to integrate one external library (libXXX.a) to dmai application video_encode_rtp(dmai_2_20_00_15/packages/ti/sdo/dmai/apps/video_encode_rtp, DVSDK4.02 ). What are the correct steps? 

Here are the steps I did.

1. Copy libXXX.a and XXX.h to video_encode_rtp;

2. In the Makefile, Add the following line in the header:

    LD_FLAGS = -lXXX -L .

3. The undefined reference errors still can be met when to build the application.

4. I manually added the followings in the auto-generated file linker.cmd and then the building is passed the executable binary can run correctly.

INPUT (

   absolute_path/libXXX.a  //the added line

...

)

I know the step 4 is a hack and the change is remove when clean and build all again. So I what to know what are the correct steps to integrate a external library into DMAI application.

Thanks a lot!