This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How do I get gcc onto the psp?

Hello

I have an AM335x EVM.  I would like to compile packages natively on the board, but I cannot find gcc in the file system image 'ti-sdk-am335x-evm-05.04.01.00".  How do I get it installed so I can run gcc, make, etc. when I am logged in to the EVM through the serial port?

I need to do this because using CCS to cross compile is fine for some programs, and I have been using it, but some packages have complicated make files and installs that really need to be run natively on the machine.

Thanks for the help.