This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

possible errors in default linker command file DM6446.cmd



Hello,

I was looking at the default linker command file DM6446.cmd in Code Composer version 5.2.0.00069. These two lines appear incorrect:

DSP_L1D:       o = 0x00F04000  l = 0x0000B000  /* 48kB DSP L1 Data RAM */

SH_DSP_L1D:    o = 0x11F04000  l = 0x0000B000  /* 48kB Shared DSP L1 Data RAM */

The defined lengths "0x0000B000" are equivalent to 44 kB, which does not match the 48 kB listed in the comment and also the TMS320DM6446 datasheet. I believe the correct lengths should be "0x0000C000"

Can someone please confirm if this is a mistake?

Thanks,

Bryan Brudevold