This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168: Problem with shared memory allocation.



Hi,

I am trying to allocate shared memory from IPC_SR_FRAME_BUFFERS region. I am able to do it with single process but I want to allocate memory from two separate process at the same time.

Below is the scenario and its behavior (I hope I will be able to explain it clearly) . I created two sample application to minimize the scope:

  • Sample Application-1 (Process-1) : which does following:
  1. Init OMX using OMX_Init();
  2. Allocate heap using SharedRegion_getHeap()
  3. Allocate buffer using Memory_alloc()
  4. Wait infinite using while (1)
  5. Deinit OMX
  • Sample Application-2 (Process-2) : which does following:
  1. Allocate heap using SharedRegion_getHeap()
  2. Allocate buffer using Memory_alloc()

Scenario-1

  1. Run Sample Application-1 in background - Memory allocated successfully.
  2. Again Run Sample Application-1 - OMX Failed to initialize and gives errors - Attached log -
    Assertion at Line no: 419 in /swcoe/sdk/cm/netra/arago-tmp/work/dm816x-evm-none-linux-gnueabi/ti-syslink-2_00_05_85-r4i/syslink_2_00_05_85/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/ipc/hlos/knl/Linux/MessageQDrv.c: (cargs.args.create.handle != NULL) : failed
    Assertion at Line no: 419 in /swcoe/sdk/cm/netra/arago-tmp/work/dm816x-evm-none-linux-gnueabi/ti-syslink-2_00_05_85-r4i/syslink_2_00_05_85/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/ipc/hlos/knl/Linux/MessageQDrv.c: (cargs.args.create.handle != NULL) : failed
    Assertion at Line no: 419 in /swcoe/sdk/cm/netra/arago-tmp/work/dm816x-evm-none-linux-gnueabi/ti-syslink-2_00_05_85-r4i/syslink_2_00_05_85/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/ipc/hlos/knl/Linux/MessageQDrv.c: (cargs.args.create.handle != NULL) : failed
    Assertion at Line no: 1244 in /home/krunal/release_014/ezsdk_504/component-sources/syslink_2_00_05_85/packages/ti/syslink/ipc/hlos/usr/MessageQ.c: (handle != NULL) : failed
    Assertion at Line no: 700 in /home/krunal/release_014/ezsdk_504/component-sources/syslink_2_00_05_85/packages/ti/syslink/ipc/hlos/usr/MessageQ.c: (queueId != MessageQ_INVALIDMESSAGEQ) : failed
    ServiceMgr_prime: MessageQ_put failed: status = 0xfffffffe
    Assertion at Line no: 1244 in /home/krunal/release_014/ezsdk_504/component-sources/syslink_2_00_05_85/packages/ti/syslink/ipc/hlos/usr/MessageQ.c: (handle != NULL) : failed
    Assertion at Line no: 700 in /home/krunal/release_014/ezsdk_504/component-sources/syslink_2_00_05_85/packages/ti/syslink/ipc/hlos/usr/MessageQ.c: (queueId != MessageQ_INVALIDMESSAGEQ) : failed
    ServiceMgr_prime: MessageQ_put failed: status = 0xfffffffe
    Assertion at Line no: 1244 in /home/krunal/release_014/ezsdk_504/component-sources/syslink_2_00_05_85/packages/ti/syslink/ipc/hlos/usr/MessageQ.c: (handle != NULL) : failed
    Assertion at Line no: 700 in /home/krunal/release_014/ezsdk_504/component-sources/syslink_2_00_05_85/packages/ti/syslink/ipc/hlos/usr/MessageQ.c: (queueId != MessageQ_INVALIDMESSAGEQ) : failed
    ServiceMgr_prime: MessageQ_put failed: status = 0xfffffffe
    Assertion at Line no: 1244 in /home/krunal/release_014/ezsdk_504/component-sources/syslink_2_00_05_85/packages/ti/syslink/ipc/hlos/usr/MessageQ.c: (handle != NULL) : failed
    Assertion at Line no: 700 in /home/krunal/release_014/ezsdk_504/component-sources/syslink_2_00_05_85/packages/ti/syslink/ipc/hlos/usr/MessageQ.c: (queueId != MessageQ_INVALIDMESSAGEQ) : failed
    ServiceMgr_prime: MessageQ_put failed: status = 0xfffffffe
    Assertion at Line no: 1244 in /home/krunal/release_014/ezsdk_504/component-sources/syslink_2_00_05_85/packages/ti/syslink/ipc/hlos/usr/MessageQ.c: (handle != NULL) : failed
    Assertion at Line no: 700 in /home/krunal/release_014/ezsdk_504/component-sources/syslink_2_00_05_85/packages/ti/syslink/ipc/hlos/usr/MessageQ.c: (queueId != MessageQ_INVALIDMESSAGEQ) : failed
    ServiceMgr_prime: MessageQ_put failed: status = 0xfffffffe
    Assertion at Line no: 1244 in /home/krunal/release_014/ezsdk_504/component-sources/syslink_2_00_05_85/packages/ti/syslink/ipc/hlos/usr/MessageQ.c: (handle != NULL) : failed
    ServiceMgr_rxThreadFxn: bind() failed with errno = 98
    Assertion at Line no: 766 in /home/krunal/release_014/ezsdk_504/component-sources/syslink_2_00_05_85/packages/ti/syslink/ipc/hlos/usr/MessageQ.c: (handle != NULL) : failed
  • Query: Does OMXInit is can be done only once? Isn't it re-entrant?

Scenario-2

  1. Run Sample Application-1 in background - Memory allocated successfully.
  2. Run Sample Application-2 - Allocation failed with error - Attached log -
    Assertion at Line no: 1081 in /home/krunal/release_014/ezsdk_504/component-sources/syslink_2_00_05_85/packages/ti/syslink/ipc/hlos/usr/SharedRegion.c: (id < SharedRegion_module->cfg.numEntries) : failed
  • Query: Is it necessary to call OMXInit() before memory allocation from SharedRegion? Should both OMXInit() and Shared region allocation be done from same process context ?

Query:

How can I allocate memory from shared region when the OMXInit() is done from separate process?

Any help will be highly appreciated.!

Regards,

Krunal