This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365 CMEMK.c error



Hello,

 

I am getting cmemk.c error on IPNCDM365 hardware with 2.1 and 2.6 firmware versions. Boot log for firmware version 2.6 is as below


DM36x initialization passed!
TI UBL Base Version: 1.50
Boot Loader BootMode = NAND
Starting NAND Copy...
Valid magicnum, 0xA1ACED66, found in block 0x00000008.
Boot Mode Task Completed

IPNC UBL Version: 1.1.0
Platform: DM365

Reset RTC Fail..

Jumping to entry point at 0x81080000

U-Boot 1.3.4 (Dec  9 2010 - 17:45:52) DM365-IPNC-1.0.1

I2C:   ready
DRAM:  128 MB
NAND:  NAND device: Manufacturer ID: 0xec, Chip ID: 0x75 (Samsung NAND 32MiB 3,3V 8-bit)
Bad block table found at page 65504, version 0x00
Bad block table found at page 65472, version 0x00
32 MiB
In:    serial
Out:   serial
Err:   serial
ARM Clock :- 297MHz
DDR Clock :- 270MHz
Ethernet PHY: GENERIC @ 0x01
Hit any key to stop autoboot:  4 3 2 1 0

NAND read: device 0 offset 0x400000, size 0xe00000
 14680064 bytes read: OK

Loading from NAND 32MiB 3,3V 8-bit, offset 0x200000
   Image Name:   Linux-2.6.18_pro500-davinci_IPNC
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    1818424 Bytes =  1.7 MB
   Load Address: 80008000
   Entry Point:  80008000
## Booting kernel from Legacy Image at 80700000 ...
   Image Name:   Linux-2.6.18_pro500-davinci_IPNC
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    1818424 Bytes =  1.7 MB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

Linux version 2.6.18_pro500-davinci_IPNC_DM368_2.6.0 (root@localhost.localdomain) (gcc version 4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 PREEMPT Fri Jul 8 03:42:00 CST 2011
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
Machine: DaVinci DM365 IPNC
Memory policy: ECC disabled, Data cache writeback
DaVinci DM0365 variant 0x8
PLL0: fixedrate: 24000000, commonrate: 135000000, vpssrate: 270000000
PLL0: vencrate_sd: 27000000, ddrrate: 270000000 mmcsdrate: 49090909
PLL1: armrate: 297000000, voicerate: 118800000, vencrate_hd: 74250000
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Built 1 zonelists.  Total pages: 12288
Kernel command line: mem=48M console=ttyS1,115200n8 root=/dev/ram0 rw initrd=0x82000000,14M ip=off eth=00:0C:13:A5:DE:D1
PID hash table entries: 256 (order: 8, 1024 bytes)
Clock event device timer0_0 configured with caps set: 07
Console: colour dummy device 80x30
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory: 48MB = 48MB total
Memory: 30336KB available (3117K code, 647K data, 176K init)
Security Framework v1.0.0 initialized
Capability LSM initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
checking if image is initramfs...it isn't (bad gzip magic numbers); looks like an initrd
Freeing initrd memory: 14336K
NET: Registered protocol family 16
DaVinci: 104 gpio irqs
MUX: initialized GPIO20
MUX: initialized I2C_SCL
Generic PHY: Registered new driver
ch0 default output "COMPOSITE", mode "NTSC"
VPBE Encoder Initialized
SCSI subsystem initialized
NET: Registered protocol family 2
IP route cache hash table entries: 512 (order: -1, 2048 bytes)
TCP established hash table entries: 2048 (order: 1, 8192 bytes)
TCP bind hash table entries: 1024 (order: 0, 4096 bytes)
TCP: Hash tables configured (established 2048 bind 1024)
TCP reno registered


 ***davinci_spi_board_init()!<6>

 ***davinci_spi_board_init_End(0)!<5>VFS: Disk quotas dquot_6.5.1
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
squashfs: version 3.1 (2006/08/19) Phillip Lougher
JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.
yaffs Jul  8 2011 03:38:59 Installing.
SGI XFS with no debug enabled
Initializing Cryptographic API
io scheduler noop registered
io scheduler anticipatory registered (default)
LTT : ltt-facilities init
LTT : ltt-facility-core init in kernel
DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfbc20000 (irq = 40) is a 16550A
serial8250.0: ttyS1 at MMIO map 0x1d06000 mem 0xfbd06000 (irq = 41) is a 16550A
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
Linux video capture interface: v2.00
Trying to register davinci display video device.
layer=c10fca00,layer->video_dev=c10fcb60
Trying to register davinci display video device.
layer=c10fc800,layer->video_dev=c10fc960
davinci_init:DaVinci V4L2 Display Driver V1.0 loaded
i2c /dev entries driver
nand_davinci nand_davinci.0: Using 4-bit hardware ECC
NAND device: Manufacturer ID: 0xec, Chip ID: 0x75 (Samsung NAND 32MiB 3,3V 8-bit)
Creating 6 MTD partitions on "nand_davinci.0":
0x00000000-0x00080000 : "bootloader"
0x00080000-0x00200000 : "params"
0x00200000-0x00400000 : "kernel"
0x00400000-0x01400000 : "filesystem1"
0x01400000-0x01600000 : "filesystem2"
0x01600000-0x02000000 : "Calibration"
nand_davinci nand_davinci.0: hardware revision: 2.3
MUX: initialized SPI0_SCLK
MUX: initialized SPI0_SDO)
dm_spi.0: davinci SPI Controller driver at 0xc3866000 (irq = 42) use_dma=0
rtc_davinci_dm365 rtc_davinci_dm365.0: rtc intf: proc
rtc_davinci_dm365 rtc_davinci_dm365.0: rtc intf: dev (254:0)
rtc_davinci_dm365 rtc_davinci_dm365.0: rtc core: registered rtc_davinci_dm365 as rtc0
rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).
ASoC version 0.13.1
CQ0093 Voice Codec 0.1
asoc: cq93vc <-> davinci-vcif mapping ok
ALSA device list:
  #0: On-chip voice codec (cq93vc)
IPv4 over IPv4 tunneling driver
TCP bic registered
NET: Registered protocol family 1
NET: Registered protocol family 17
rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

rtc wait time out !!!!!

Time: timer0_1 clocksource has been installed.
Clock event device timer0_0 configured with caps set: 08
Switched to high resolution mode on CPU 0
rtc_davinci_dm365 rtc_davinci_dm365.0: setting the system clock to 2000-09-14 01:01:01 (968893261)
RAMDISK: cramfs filesystem found at block 0
RAMDISK: Loading 13712KiB [1 disk] into ram disk...done.
VFS: Mounted root (cramfs filesystem) readonly.
Freeing init memory: 176K

INIT: version 2.86 booting

0
mkdir: Cannot create directory `/dev/.test': Read-only file system
Starting the hotplug events dispatcher: udevd.
Synthesizing the initial hotplug events...done.
Waiting for /dev to be fully populated...done.
0
CSL: Module install successful, device major num = 253
CSL: Module version 0.10.00, built on Jul  8 2011 03:44:40
I2C: Module install successful, device major num = 252
DMA: Module install successful, device major num = 251
DRV: Module install successful
DRV: Module built on Jul  8 2011 03:44:42
DRV: EDMACC.QUEPRI  = 00002777
DRV: SYSTEM.MSTPRI0 = 00440022
DRV: SYSTEM.MSTPRI1 = 00000344
DRV: ISP.BCR        = 00000002
DRV: SYSTEM.MISC = 00000399
CMEMK module: built on Jul  8 2011 at 03:44:11
  Reference Linux version 2.6.18
  File /home/user/workdir/dvsdk_2_10_01_18/linuxutils_2_24_03/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c

after this program don't proceed further. If I load same files on other cards it works fine. Here I am getting hint that there might be some error related to memory. But DDR and NAND flash  aer passing test programs. I have replaced NAND flash and DDR chip just to check one of the possibilities but problem not solved

Please suggest possible solution for this.