This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi all
we have our custom board based on omap3530 soc..
the board has been successfully booted with omap-linux-3.1 and USB is working properly..
but the problem is when we try to boot the rowboat gingerbread with rowboat-kernel-2.6.37 the USB is not working
acutlly we tried to measure the voltages near the hub but in android it is not coming.. (in angstrom linux it is coming)
the usb led is ON while booting on both android and linux.
we have taken reference design from BBxm and the power ic is tps65950..
log cat has been attachd..
kindly help us to resolve this issue
thank u
40W Texas Instruments X-Loader 1.51 (Apr 21 2011 - 15:20:42) Beagle xM Rev A Starting X-loader on MMC Reading boot sector 213412 Bytes Read from MMC Starting OS Bootloader from MMC... Starting OS Bootloader... U-Boot 2010.06 (Apr 21 2011 - 15:12:08) OMAP3430/3530-GP ES3.1, CPU-OPP2 L3-165MHz OMAP3 Beagle board + LPDDR/NAND I2C: ready DRAM: 256 MiB NAND: HW ECC [Kernel/FS layout] selected 512 MiB *** Warning - bad CRC or NAND, using default environment In: serial Out: serial Err: serial Beagle xM Rev A Die ID #1a44000400000000040373051200901e Hit any key to stop autoboot: 10 9 8 7 6 5 4 3 2 1 0 mmc1 is available reading boot.scr 476 bytes read Running bootscript from mmc ... ## Executing script at 82000000 reading uImage 2870028 bytes read ***** Kernel: /dev/mmcblk0p1/uImage ***** ***** RootFS: /dev/mmcblk0p2 ***** ## Booting kernel from Legacy Image at 80200000 ... Image Name: Linux-2.6.37-g1236e9f-dirty Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 2869964 Bytes = 2.7 MiB Load Address: 80008000 Entry Point: 80008000 Verifying Checksum ... OK Loading Kernel Image ... OK OK Starting kernel ... Uncompressing Linux... done, booting the kernel. Linux version 2.6.37-g1236e9f-dirty (root@rtsg1) (gcc version 4.4.1 (Sourcery G++ Lite 2010q1-202) ) #16 Wed Jul 25 17:09:00 IST 2012 CPU: ARMv7 Processor [411fc083] revision 3 (ARMv7), cr=10c53c7f CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache Machine: OMAP3 Beagle Board Reserving 8388608 bytes SDRAM for VRAM Memory policy: ECC disabled, Data cache writeback OMAP3430/3530 ES3.1 (l2cache iva sgx neon isp 720mhz ) SRAM: Mapped pa 0x40200000 to va 0xfe400000 size: 0x10000 Built 1 zonelists in Zone order, mobility grouping on. Total pages: 62976 Kernel command line: console=ttyO2,115200n8 androidboot.console=ttyO2 mem=256M root=/dev/mmcblk0p2 rw rootfstype=ext3 rootdelay=1 init=/init ip=off omap_vout.vid1_static_vrfb_alloc=y vram=8M omapfb.vram=0:8M omapdss.def_disp=dvi omapfb.mode=dvi:1024x768-16 PID hash table entries: 1024 (order: 0, 4096 bytes) Dentry cache hash table entries: 32768 (order: 5, 131072 bytes) Inode-cache hash table entries: 16384 (order: 4, 65536 bytes) Memory: 248MB = 248MB total Memory: 244964k/244964k available, 17180k reserved, 0K highmem Virtual kernel memory layout: vector : 0xffff0000 - 0xffff1000 ( 4 kB) fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) DMA : 0xffc00000 - 0xffe00000 ( 2 MB) vmalloc : 0xd0800000 - 0xf8000000 ( 632 MB) lowmem : 0xc0000000 - 0xd0000000 ( 256 MB) modules : 0xbf000000 - 0xc0000000 ( 16 MB) .init : 0xc0008000 - 0xc003b000 ( 204 kB) .text : 0xc003b000 - 0xc0581000 (5400 kB) .data : 0xc0582000 - 0xc05c85c0 ( 282 kB) NR_IRQS:409 Clocking rate (Crystal/Core/MPU): 26.0/331/500 MHz Reprogramming SDRC clock to 331882352 Hz IRQ: Found an INTC at 0xfa200000 (revision 4.0) with 96 interrupts Total of 96 interrupts on 1 active controller GPMC revision 5.0 Trying to install interrupt handler for IRQ402 Trying to install interrupt handler for IRQ403 Trying to install interrupt handler for IRQ404 Trying to install interrupt handler for IRQ405 Trying to install interrupt handler for IRQ406 Trying to install interrupt handler for IRQ407 Trying to install interrupt handler for IRQ408 Trying to install type control for IRQ409 Trying to set irq flags for IRQ409 OMAP clockevent source: GPTIMER1 at 32768 Hz Console: colour dummy device 80x30 Calibrating delay loop... 499.92 BogoMIPS (lpj=1949696) pid_max: default: 32768 minimum: 301 Security Framework initialized Mount-cache hash table entries: 512 CPU: Testing write buffer coherency: ok regulator: core version 0.5 regulator: dummy: NET: Registered protocol family 16 OMAP GPIO hardware version 2.5 OMAP GPIO hardware version 2.5 OMAP GPIO hardware version 2.5 OMAP GPIO hardware version 2.5 OMAP GPIO hardware version 2.5 OMAP GPIO hardware version 2.5 omap_mux_init: Add partition: #1: core, flags: 0 OMAP3 Beagle Rev: xM Found NAND on CS0 Registering NAND on CS0 Unable to get DVI reset GPIO hw-breakpoint: debug architecture 0x4 unsupported. OMAP DMA hardware revision 4.0 bio: create slab <bio-0> at 0 SCSI subsystem initialized usbcore: registered new interface driver usbfs usbcore: registered new interface driver hub usbcore: registered new device driver usb omap_i2c omap_i2c.1: bus 1 rev3.12 at 2600 kHz twl4030: PIH (irq 7) chaining IRQs 368..375 twl4030: power (irq 373) chaining IRQs 376..383 twl4030: gpio (irq 368) chaining IRQs 384..4 regulator: VUSB1V5: 1500 mV normal standby regulator: VUSB1V8: 1800 mV normal standby regulator: VUSB3V1: 3100 mV normal standby twl4030_usb twl4030_usb: Initialized TWL4030 USB module regulator: VMMC1: 1850 <--> 3150 mV at 3000 mV normal standby regulator: VDAC: 1800 mV normal standby regulator: VDVI: 1800 mV normal standby regulator: VSIM: 1800 <--> 3000 mV at 1800 mV normal standby regulator: VAUX3: 1800 mV normal standby regulator: VAUX4: 1800 mV normal standby omap_i2c omap_i2c.2: bus 2 rev3.12 at 400 kHz omap_i2c omap_i2c.3: bus 3 rev3.12 at 100 kHz Advanced Linux Sound Architecture Driver Version 1.0.23. cfg80211: Calling CRDA to update world regulatory domain Switching to clocksource 32k_counter musb-hdrc: version 6.0, otg (peripheral+host), debug=0 musb-hdrc musb-hdrc.0: dma type: dma-inventra musb-hdrc musb-hdrc.0: USB OTG mode controller at fa0ab000 using DMA, IRQ 92 NET: Registered protocol family 2 IP route cache hash table entries: 2048 (order: 1, 8192 bytes) TCP established hash table entries: 8192 (order: 4, 65536 bytes) TCP bind hash table entries: 8192 (order: 3, 32768 bytes) TCP: Hash tables configured (established 8192 bind 8192) TCP reno registered UDP hash table entries: 256 (order: 0, 4096 bytes) UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) NET: Registered protocol family 1 NetWinder Floating Point Emulator V0.97 (double precision) platform iva.0: Enabled OPP corresponding to 720MHz omap-iommu omap-iommu.0: isp registered OMAP35x Linux PSP version 04.02.00.07 (OMAP3BEAGLE) ashmem: initialized VFS: Disk quotas dquot_6.5.2 Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) JFFS2 version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc. msgmni has been set to 478 io scheduler noop registered io scheduler deadline registered io scheduler cfq registered (default) OMAP DSS rev 2.0 OMAP DISPC rev 3.0 OMAP VENC rev 2 OMAP DSI rev 1.0 Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled omap_uart.0: ttyO0 at MMIO 0x4806a000 (irq = 72) is a OMAP UART0 omap_uart.1: ttyO1 at MMIO 0x4806c000 (irq = 73) is a OMAP UART1 omap_uart.2: ttyO2 at MMIO 0x49020000 (irq = 74) is a OMAP UART2 console [ttyO2] enabled brd: module loaded loop: module loaded mtdoops: mtd device (mtddev=name/number) must be supplied omap2-nand driver initializing NAND device: Manufacturer ID: 0x2c, Chip ID: 0xbc (Micron ) Creating 5 MTD partitions on "omap2-nand.0": 0x000000000000-0x000000080000 : "X-Loader" 0x000000080000-0x000000260000 : "U-Boot" 0x000000260000-0x000000280000 : "U-Boot Env" 0x000000280000-0x000000680000 : "Kernel" 0x000000680000-0x000020000000 : "File System" OneNAND driver initializing PPP generic driver version 2.4.2 PPP Deflate Compression module registered PPP BSD Compression module registered PPP MPPE Compression module registered NET: Registered protocol family 24 SLIP: version 0.8.4-NET3.019-NEWTTY (dynamic channels, max=256). CSLIP: code copyright 1989 Regents of the University of California. usbcore: registered new interface driver asix usbcore: registered new interface driver cdc_ether usbcore: registered new interface driver smsc95xx usbcore: registered new interface driver net1080 usbcore: registered new interface driver cdc_subset usbcore: registered new interface driver zaurus ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver ehci-omap.0 supply hsusb0 not found, using dummy regulator ehci-omap.0 supply hsusb1 not found, using dummy regulator ehci-omap ehci-omap.0: OMAP-EHCI Host Controller ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 1 ehci-omap ehci-omap.0: irq 77, io mem 0x48064800 ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00 usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 usb usb1: Product: OMAP-EHCI Host Controller usb usb1: Manufacturer: Linux 2.6.37-g1236e9f-dirty ehci_hcd usb usb1: SerialNumber: ehci-omap.0 hub 1-0:1.0: USB hub found hub 1-0:1.0: 3 ports detected Initializing USB Mass Storage driver... usbcore: registered new interface driver usb-storage USB Mass Storage support registered. usbcore: registered new interface driver usbserial USB Serial support registered for generic usbcore: registered new interface driver usbserial_generic usbserial: USB Serial Driver core USB Serial support registered for cp210x usbcore: registered new interface driver cp210x cp210x: v0.09:Silicon Labs CP210x RS232 serial adaptor driver USB Serial support registered for GSM modem (1-port) usbcore: registered new interface driver option option: v0.7.2:USB Driver for GSM modems USB Serial support registered for pl2303 usbcore: registered new interface driver pl2303 pl2303: Prolific PL2303 USB to serial adaptor driver android init android_probe pdata: c05920dc android_bind android_usb gadget: android_usb ready musb-hdrc musb-hdrc.0: MUSB HDRC host driver musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2 usb usb2: New USB device found, idVendor=1d6b, idProduct=0002 usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 usb usb2: Product: MUSB HDRC host driver usb usb2: Manufacturer: Linux 2.6.37-g1236e9f-dirty musb-hcd usb usb2: SerialNumber: musb-hdrc.0 hub 2-0:1.0: USB hub found hub 2-0:1.0: 1 port detected f_adb init android_register_function adb f_mass_storage init fsg_probe pdev: c0591f20, pdata: c0592134 android_register_function usb_mass_storage adb_bind_config android_usb gadget: Mass Storage Function, version: 2009/09/11 android_usb gadget: Number of LUNs=1 lun0: LUN: removable file: (no medium) input: gpio-keys as /devices/platform/gpio-keys/input/input0 input: twl4030_pwrbutton as /devices/platform/omap/omap_i2c.1/i2c-1/1-0049/twl4030_pwrbutton/input/input1 using rtc device, twl_rtc, for alarms twl_rtc twl_rtc: rtc core: registered twl_rtc as rtc0 twl_rtc twl_rtc: Power up reset detected. twl_rtc twl_rtc: Enabling TWL-RTC. i2c /dev entries driver Linux media interface: v0.10 Linux video capture interface: v2.00 omap3isp supply VDD_CSIPHY1 not found, using dummy regulator omap3isp supply VDD_CSIPHY2 not found, using dummy regulator omap3isp omap3isp: Revision 2.0 found omap-iommu omap-iommu.0: isp: version 1.1 omap_i2c omap_i2c.2: controller timed out mt9v113 2-003c: chip id mismatch read 0x0, expecting 0x2280 isp_register_subdev_group: Unable to register subdev mt9v113 OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec twl4030_wdt twl4030_wdt: Failed to register misc device twl4030_wdt: probe of twl4030_wdt failed with error -16 device-mapper: uevent: version 1.0.3 device-mapper: ioctl: 4.18.0-ioctl (2010-06-29) initialised: dm-devel@redhat.com usbcore: registered new interface driver usbhid usbhid: USB HID core driver logger: created 64K log 'log_main' logger: created 256K log 'log_events' logger: created 64K log 'log_radio' logger: created 64K log 'log_system' usbcore: registered new interface driver snd-usb-audio OMAP3 Beagle/Devkit8000 SoC init asoc: twl4030-hifi <-> omap-mcbsp-dai.1 mapping ok ALSA device list: #0: omap3beagle oprofile: hardware counters not available oprofile: using timer interrupt. TCP cubic registered Initializing XFRM netlink socket NET: Registered protocol family 17 NET: Registered protocol family 15 lib80211: common routines for IEEE802.11 drivers Registering the dns_resolver key type VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 1 ThumbEE CPU extension supported. Power Management for TI OMAP3. smartreflex smartreflex.0: omap_sr_probe: SmartReflex driver initialized smartreflex smartreflex.1: omap_sr_probe: SmartReflex driver initialized SmartReflex Class3 initialized clock: disabling unused clocks to save power platform iva.0: omap_voltage_scale: Already at the requestedrate 360000000 platform mpu.0: omap_voltage_scale: Already at the requestedrate 500000000 regulator_init_complete: incomplete constraints, leaving VDAC on twl_rtc twl_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800) omap_vout omap_vout: Buffer Size = 3686400 omap_vout omap_vout: : registered and initialized video device 15 omap_vout omap_vout: Buffer Size = 3686400 omap_vout omap_vout: : registered and initialized video device 16 Waiting 1sec before mounting root device... mmc0: host does not support reading read-only switch. assuming write-enable. mmc0: new high speed SDHC card at address 3150 mmcblk0: mmc0:3150 SD04G 3.69 GiB mmcblk0: p1 p2 EXT3-fs: barriers not enabled kjournald starting. Commit interval 5 seconds EXT3-fs (mmcblk0p2): warning: maximal mount count reached, running e2fsck is recommended EXT3-fs (mmcblk0p2): using internal journal EXT3-fs (mmcblk0p2): recovery complete EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode VFS: Mounted root (ext3 filesystem) on device 179:2. Freeing init memory: 204K init: cannot open '/initlogo.rle' init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead. init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery' enabling adb adb_open # warning: `zygote' uses 32-bit capabilities (legacy support in use) tps65950