This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Initializing SPI-Flash with boot-code on C6742 without CCS

Hello everybody,

we are doing a design for the C6742 with a SPI-Flash for boot-code.

During development we will use CCSv5 with a XDS100 JTAG Interface. With this tools I can load the SPI-Flash, am I right?

But in production this method is not applicable. How can I program the SPI-Flash over JTAG (with or without XDS100) without CCS? I found a SDFLASH utility from SpectrumDigital. Does this utility work with a XDS100?

For C6747/C6748 I saw another method over UART. Is this also possible with C6742?

Thanks in advance,

Bernd Büttner