This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BCP Test Project not working

Hello,

I use CCS 5.2 and MCSDK 2_00_09_21 on a C6670L EVM connected with XDS100usb. When I run the BCP Test Project, the external protocoll related lte, wcdma and wimax ".dat" files cannot be included why I think I get the following console output:

[C66xx_0] **************************************************
[C66xx_0] *************** BCP Testing Start ***************
[C66xx_0] **************************************************
[C66xx_0] Using BCP Driver version: 0x1000009 Version Info: BCP Driver Revision: 01.00.00.09:Aug  1 2012:15:01:45
[C66xx_0] [Core 0]: L1D cache size 0. L2 cache size 0.
[C66xx_0] [Core 0]: BCP instance 0 successfully initialized
[C66xx_0] [Core 0]: BCP driver successfully opened
[C66xx_0] Global FDQ 877 successfully setup with 64 descriptors
[C66xx_0]
[C66xx_0] -------------- Rel99 DL Test Start ---------------
[C66xx_0] Rx FDQ 736 successfully setup with 48 descriptors
[C66xx_0] Flow 0 opened to send data to RxQ: 900
[C66xx_0] Tx FDQ 737 successfully setup with 16 descriptors
[C66xx_0] Error building/sending R99 DL packets
[C66xx_0] WCDMA Rel-99 DL Test:    FAILED
[C66xx_0]
[C66xx_0] -------------- Rel99 UL Test Start ---------------
[C66xx_0] Rx FDQ 736 successfully setup with 48 descriptors
[C66xx_0] Flow 0 opened to send data to RxQ: 900
[C66xx_0] Tx FDQ 737 successfully setup with 16 descriptors
[C66xx_0] Error reading test vectors/populating R99 UL packet
[C66xx_0] WCDMA Rel-99 UL Test:    FAILED
[C66xx_0]
[C66xx_0] -------------- WCDMA DL Test Start --------------
[C66xx_0] Rx FDQ 736 successfully setup with 62 descriptors
[C66xx_0] Flow 0 opened to send data to RxQ: 900
[C66xx_0] Error opening Tx FDQ
[C66xx_0]
[C66xx_0] -------------- WCDMA UL Test Start --------------
[C66xx_0] Error opening Tx FDQ
[C66xx_0]
[C66xx_0] -------------- WiMax DL Test Start ---------------
[C66xx_0] Error opening Rx FDQ
[C66xx_0]
[C66xx_0] -------------- WiMax UL Test Start ---------------
[C66xx_0] Error opening Rx FDQ
[C66xx_0]
[C66xx_0] -------------- LTE UL Test Start --------------
[C66xx_0] Error opening Tx FDQ
[C66xx_0]
[C66xx_0] -------------- LTE DL Test Start --------------
[C66xx_0] Error opening Tx FDQ
[C66xx_0]
[C66xx_0] -------------- BCP Testing Complete --------------
[C66xx_0] Num Test Failures = 2
[C66xx_0] Waiting for other cores to finish ...
[C66xx_0] **************************************************
[C66xx_0] ****************** BCP Testing End **************
[C66xx_0] **************************************************
[C66xx_0] [Core 0]: BCP Test Unloaded successfully
[C66xx_0] BcpAlloc Cnt:        205 BcpFree Cnt:    138
[C66xx_0] CppiMalloc Cnt:        1 CppiFree Cnt:    0
[C66xx_0] QmssAlloc Cnt:        0 QmssFree Cnt:    0

I appreciate any help with this issue.

Best Regards

Burak