This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bug in DM648 DAT_copy?

There is a project to demo. the use of DAT_copy like DM642 CSL API in "C:\dvsdk_1_11_00_00_DM648\edma3_lld_1_05_00\examples\CSL2_DAT_DEMO\demo\dat_demo_dm648.pjt"

 

But when I build my own project base on this demo project, use DAT_copy with other tasks and interrupts such as sdvideodigloopback_tst.pjt  in  C:\Lyrtech\EVMDM648\BSL\Example\SDVideoDigLoopBack_tst, I find the whole system will run down no longer than running one minute. I have tried many methods to prevent so, but all faild.

 

I guess this is a bug in DAT_copy of DM648, which will cause DAT_copy can't work well in the environment of many tasks and interrupts.