We have a working PCIe example using the C6678 EVM and an FPGA EVM connected through a custom PCIe backplane. Link training works fine, and we are able to write / read data to / from the FPGA from the DSP.
We are now trying to run the same example over a fiber optic PCIe link (Finisar Laserwire). We have two of custom PCIe backplanes (both verified) - one with the DSP EVM and a Laserwire adaptor board, the other with the FPGA EVM and a Laserwire adaptor board.
With this setup, the DSP never gets past the DETECT_QUIET ltssm value during link training.
Is there a way to force the DSP's PCIe state machine past the DETECT_QUITE state?
Any trouble-shooting suggestions will be greatly appreciated.
~ Andrew.