This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Static parameters

Guru 20755 points


Hello, I'm using RDK and would like to ask, when some feature can't be changed dynamically, must we then use stop/start for the chain with the changed value ? Are there eany demos for such cases ? Are there other scenarios when even stop/start can't be done and we need to load the firmware in order to change some feature ? Do you have any examples for such cases when we need to load firmware ? Regards, Ran