This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

boot hangs while/after inserting edmak module



Hello everybody,

when booting the EVMDM365 board, the boot process stops or hangs when inserting the edmak module. At least this is the last message printed out to the console. The filesystem and the kernel are booting from NAND flash and I use a JFFS2 filesystem. While booting I get several jffs2 error messages like:

"jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x027de800: 0xc030 instead"

or

"mtd->read(0x400 bytes from 0x18ae0000) returned ECC error"

The messages always come up but the boot process always worked until today...

I use the filesystem and the kernel which are delivered in DVSDK 4.02.

Regards,

Matthias