This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Cannot Apply TI SPRZ319e DPLL5 to BeagleBoard xM for USB EHCI clock drift at 26MHZ system clock



Does anyone know why I cant apply TI SPRZ319e DPLL5 setting {M=443,N=11 and M2=8} to the BBxM ??
(M/N)/M2.
This is for USB EHCI clock drift.
Only {443,11 and 4} works for the 10/100Mbps Ethernet which operates off the internal USB hub.
It seems the equation must end up equaling 10 and the Errata gives the result 5 which causes ethernet to not initialize.
I would like to apply the Errata but problems - can anyone give me some insight ??
Thanks !!