This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5515 eZDSP USB Stick Development Tool CC Connectors

Other Parts Discussed in Thread: CC1125, TMDX5515EZDSP

Hi all,

I need to know if TMDX5515EZDSP Chipcon Connectors are compatible with CC1125.

Thank you

  • Hi,

    CC1125EM schematics and layout are available here: http://www.ti.com/lit/ug/swrr097/swrr097.zip

    C5515 eZdsp schematics and layout are available here: http://support.spectrumdigital.com/boards/usbstk5515

    All of the power, ground, SPI signals, and the RESET signal are compatible, but there is a slight issue with the CC1125EM GPIO3 pin. See the RF header comparison below.

    To have SPI signals present on the P1 header, the C5515 pin multiplexing must be in PPMODE 1 or 6 (See Table 4-7. LCD Controller, SPI, UART, I2S2, I2S3, and GP[31:27, 20:18] Pin Multiplexing in C5515 datasheet)

    GP[29] is available from the LCD_D[13]/UART_CTS/GP[29]/I2S3_FS pin only when PPMODE = 2...

    So the signal present on the CC1125EM GPIO3 will actually be UART_CTS (PPMODE 1) or I2S3_FS (PPMODE 6).

    I'm not sure what the GPIO3 signal is used for, and you should double check it... but I get the feeling that the CC1125EM will work fine.

    Hope this helps,
    Mark