Other Parts Discussed in Thread: OMAP-L138, OMAPL138
Hello:
I am working on a new project with the TI OMAP-L138 and have worked previously with the TI C64xx family of processors. In my experience, the CSL for the ‘C64xx family is pretty mature and in working now with the OMAP-L138, I was hoping to find some of the same functions that are available in the ‘C64xx CSL. Specifically, I’d like to use a function on the OMAP-L138 called the “dat_copy” function, but have not been able to find it. Are there additional libraries or functions like this available for the OMAP-L138? If so, can you please tell me where to find them? Perhaps there are some third-party libraries or something that I can make use of?
Any feedback or input is welcomed and appreciated!
Thanks again!
Paul