I have connected the am335x-evm's ethernet line and the serial line to my laptop. I am able to communicate to the device over COM port and there seems to be no issues. I ran the ifconfig command on the device and eth0 is listed with an IP of 192.168.1.100. However it does not seem to connect to the linux vmware. Is there a wiki to follow to do this ssh connection over linux or ubuntu? When I try to connect I get either 'Connection Refused" or "Network is Unreachable".