This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

xds100v2 emulate on EVMDM8148 too slowly!



Hi, all:

       I want to emulate the speed of the C6000 DSP on EVMDM8148 board, there are much double mux and div calculation in my test code.

       In the debug mode, I got the CPU clock is about 1,187,500,000 clks, and it’s spent about 27 seconds. But on the other hand, I calculate the time by DSP clock which is 1,187,500,000/500/(1000*1000)=2.375s

    The gel file output like the list(in ARM):

CortexA8: Output:    ****  DM8148 ALL ADPLL INIT IS In Progress .........

CortexA8: GEL Output:    A8 ADPLLJ CLKOUT  value is  = 600

CortexA8: GEL Output:    L3  ADPLLJ CLKOUT  value is  = 200

CortexA8: GEL Output:    DSP ADPLLJ CLKOUT  value is  = 500

CortexA8: GEL Output:    DSS ADPLLJ CLKOUT  value is  = 200

CortexA8: GEL Output:    HDVICP ADPLLJ CLKOUT  value is  = 266

CortexA8: GEL Output:    SGX ADPLLJ CLKOUT  value is  = 200

CortexA8: GEL Output:    USB ADPLLJ CLKOUT  value is  = 192

CortexA8: GEL Output:    VIDEO-0 ADPLLJ CLKOUT  value is  = 54

CortexA8: GEL Output:    VIDEO-1 ADPLLJ CLKOUT  value is  = 148

CortexA8: GEL Output:    VIDEO-2/HDMI ADPLLJ CLKOUT  value is  = 148

CortexA8: GEL Output:    AUDIO ADPLLJ CLKOUT  value is  = 200

    SO, the DSP core clock at 500M! 

    How to explain this, which is TURE speed?  Thanks any relay!