This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Configuration for TPS65910A3 to support DDR3 with AM335x



Hi All,

  1. DDR3  SDRAM memory(MT4IJ128M16JT-125) design is provided  on StarterKit  EVM , 
  2. according to the TPS65910A3 datasheet, The VIO_SMPS output from the PMIC is programmed to provide the required 1.5V to the DDR3 SDRAM.

            VIO_REG SEL VIO voltage selection (DDR2) TPS65910A3A1 1.5V(DDR3)

      3 Add source code support for DDR3 SDRAM in AM335XPSP_04.06.00.08

         But  I can't find where to config the VIO_REG of  TPS6510A3 in the sourcecode of AM335xPSP_04.06.00.08.

         thanks !