I am stuck with the OMAP l138 EVM. The funny thing is that the OMAP l138 eXperimenter and EVM are quite different.
I am reading a book that is applicable to OMAP eXperimenter... but it doesn't seems to be clear for the EVM.
http://www.amazon.com/Digital-Signal-Processing-Applications-OMAP/dp/047093686X
This book said as a first example:
* Connect a line level audio source, e.g. the output from a PC sound card, to the LINE IN socket on the OMAP l138. Make sure the source is sufficiently low that it will not damage the input circuits of the AIC3106 codec.
* Connect either headphones or loudspeakers to the LINE OUT socket on the OMAP.
The problem is that in the EVM, I couldn't find the LINE IN/OUT, unless S-VIDEO IN/OUT and COMP-VIDEO IN/OUT also can serve the same way for audio and video.
All comments are highly welcome.