hi,
Now, I can connect A8 and M3 with CCS5.1 and XDS560, based on the GEL files along with the IPNC RDK Release 3.0. However, the C674x core cannot be connected successfully. If try, the following error message shown in the CCS console:
Error connecting to the target: (Error -1180 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 5.0.520.0).
The default GEL file does not support the DSP debug? How can I do for it?
B.R.