im using a 32GB external nand from hynix along with omap3530,this is in addition to POP memory...... so that i can use this 32GB nand as hard disk(mass storage) to store large files...... i have interfaced it through GPMC,all things related to hardware interfacing is finished..... now the software part comes into picture... im really stuck.... i dnt know where to start.. im planning to use CS1..... can u guide me through some article or tutorial??? pls.. :) can u pls give me a list of files i need to edit in the BSP.. im using wince BSP version 1.3