I'm using the 6670 (rev 2.0), and setup Timer0 to work as a watchdog timer for core 0. It works fine however even with the SOFT and FREE bits in EMUMGT_CLKSPD set to 0, the clock continues to count up. This makes it a bit difficult to debug things once it is initialized. Is there anything I am missing that I need to do to not get it to count up when the emulator his a break point?