This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to compile assembly code of TI's C5515 on CCS 4.3.9



Dear Team,

   Currently I am facing problem with compiling and linking assembly code on CCS 4.3.9, So request you to provide the solution asap.

Problem: I have implemented and integrated the FIR filter with order 128 in C but it is taking much time for processing, hence i am planning to use assembly.

                  I downloaded the code for TI's Medical Development Kit for C5515 and tried to integrate the filter code with my code but it is giving compilation and linking errors.

                Following code snippet  and error is given for reference.

                /*     Initilizing output as zero      */
                        asm("    *AR2 = #0");
                /* Loop count */
                   asm("    T0 = #161");
                    asm("    AC0 = #0");
               /* Loop starts */
                  asm("LOOP?    ");
                  asm("    T0 -= #1");
                  asm("    AC0 += ((*AR0-) * (*AR1+))");
                  asm("    if (T0 != #0) goto LOOP?");       
           /*     Loop ends     */
                  asm("    nop");
                  asm("    nop");
                  asm("    (*AR2+) = HI(AC0) ");
                  asm("    *AR2 = AC0 ");


  
Error Displayed by CCS :
                              [E9999] Illegal directive or mnemonic.
                              [E9999] Invalid mnemonic specified.
                              [E9999] Synatax Error.


  To avoid the problem i also tried the following

 Go to CCS – build options – compiler settings --- Runtime model options --- select assembly source language

  and tried both algebraic & mnemonic.

  But still it is showing errors for other piece of code (which was compiling fine earlier without above settings).

 So I want to know whether the code provided above is correct or not? And if it is correct then how to successfully build the project and execute it?