Hello,
We will be using TI's OMAP-L138, but we understand Sys/Bios cannot support the ARM. If we use Starterware combined with Sys/Bios will we still have the diagsnostics capabilities? Or only on the DSP?
Thanks,
Michelle
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
We will be using TI's OMAP-L138, but we understand Sys/Bios cannot support the ARM. If we use Starterware combined with Sys/Bios will we still have the diagsnostics capabilities? Or only on the DSP?
Thanks,
Michelle
Yes, but it does not have a peripheral support packge for the ARM, am I right? For peripheral support on the Arm9 I'd need to use Starterware.
Yes, you are correct. We have not tested the PSP with SYS/BIOS.
Which diagnostic capabilities are you referring to?
Todd
Hello Todd,
This is the information I got:
The following diagnostics capabilities are available…
|
Diagnostics |
Log |
Allows events to be logged and then passes those events to a Log handler. |
|
Assert |
Provides for configurable assertion diagnostics. |
|
|
Error |
Allows raising, checking, and handling errors defined by any modules. |
|
|
Timestamp |
Provides time-stamping APIs that forward calls to a platformspecific time stamper (or one provided by CCS). |
|
|
Diags |
Allows diagnostics to be enabled/disabled at either configuration- or run-time on a per-module basis. |
Hi Michelle,
Actually all of these can be used without SYS/BIOS. They are part of XDCtools (which is OS independent). You'll need to make your project a RTSC project with a .cfg file.
Todd