This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is any command support to delete the file on the SD/MMC card in u-bootloader?



Hi,

I just want to know is there any support or code or command for the delete/erase the file (abc.txt) in the SD/MMC card?

e.g : i have one file abc.txt in the SD card. I have to delete the file from the u-boot. Is there any command to delete the file.

means as i can write the file on sd card using fatwrite command , same can i delete the file using any command?

Please awaiting for reply.