Hi all
I use beagleboard-xm , and get the android pre-build images for Pre-built Images from http://software-dl.ti.com/dsps/dsps_public_sw/sdo_tii/TI_Android_DevKit/TI_Android_GingerBread_2_3_4_DevKit_2_1/index_FDS.html
In my application, I want to use the sendevent to finish the following work, move the Cursor to the position, and click.
The code used to move the cursor
sendevent /dev/input/event3 2 0 4
sendevent /dev/input/event3 0 0 0
sendevent /dev/input/event3 2 1 5
sendevent /dev/input/event3 0 0 0
The code used to generate a click
sendevent /dev/input/event3 4 4 589825
sendevent /dev/input/event3 1 272 1
sendevent /dev/input/event3 0 0 0
sendevent /dev/input/event3 4 4 589825
sendevent /dev/input/event3 1 272 0
sendevent /dev/input/event3 0 0 0
But they all didn't work!
I test this code in a MTK-android board, it can work correctly!
Another question:
I download the source code of Android GINGERBREAD 2.3.4, and want to re-compile the filesystem. I following the instruction of document TI-Android-GingerBread-2.3.4-DevKit-2.1 DeveloperGuide.pdf.
use "make TARGET_PRODUCT= beagleboard OMAPES=5.x -j8", But about 14h later , the compiler still compiling, why use so long time?