This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM387 dual mac mode

Hi Champs,

 

we  want to use AM387 with Win Compect 7 in dual mac mode(to enable one default Ethernet and on EtherCAT Master port).

Which modifikations we have to do on the driver?

We have seen that per default only two DMAQueues are enabled(RX/TX).

 

Are EMAC and DMA drivers in kernel or usermode?

Can we use without Kernel sync?

 

Thanks and Best Regards

David