I have developed a test program for an I/O card I designed using CCS version 5.2. My micro controller is an AM335x device. The hardware platform is a BeagleBone card. I have the program completely check-out and functional. I downloaded the program to debug and check it out using CCS via the USB port to the BeagleBone. Now I want to install the program on the BeagleBone’s SD card and execute it. The BeagleBone operating system is Linux.
What conversion if any do I need to do to load it on the SD disk of the BeagleBone? I am having difficult getting an answer to this issue.
Do I need to convert the .out output from CCS to something else?
Who can tell me what to do?
The hardware has been complete for about four month and I have not been able to find out how to get the control program onto the BeagleBone’s SD drive.
Regards
Larry