Other Parts Discussed in Thread: TVP5158
Hi all:
I am using DM6437 connect with TVP5158 decoder to get 2-ch D1 image(line-interleaved mode). I refer to the examle of in the path of \dvsdk_1_01_00_15\psp_1_00_02_00\pspdrivers.....\loopback\.But when it runs into :
if(IOM_COMPLETED != FVID_exchange(CcdcHandle,&FBAddr))
{
VPSS_DBG("VPSS :CCDC Exchange.......FAILED \r\n");
}
FVID_exchange() faied.
I config the CCDC like this:
PSP_VPFECcdcConfigParams ccdcParams =
{
FVID_CCDC_YCBCR_8, /* dataFlow */
FVID_FRAME_MODE, /* ffMode */
1250,// 480, /* height */
736, /* width */
(736 *2), /* pitch */
0, /* horzStartPix */
0, /* vertStartPix */
NULL, /* appCallback */
{
PSP_VPFE_TVP5158_Open, /* extVD Fxn */
PSP_VPFE_TVP5158_Close,
PSP_VPFE_TVP5158_Control,
},
0 /*segId */
};
I have two questions :
1. Why did FVID_exchange() fail?How can I corrected?
2. I found if the input mode of VPFE is configed FVID_FIELD_MODE,FVID_creat() will fail .But if it is configed FVID_FRAME_MODE,the FVID_exchange will fail. the data stream of input should be FVID_FIELD_MODE.
Could you help me?