Hi All,
I Configured wvdial(.ipk file)and all dependency files on client machine. after that i am giving command which wvdial , then its given /usr/bin/wvdial. that means i installed succefully wvdial.
Then i am giving wvdial on terminal, i am getting the following msg.
/ # wvdial
--> WvDial: Internet dialer version 1.60
--> Warning: section [Dialer Defaults] does not exist in wvdial.conf.
--> Cannot open /dev/modem: No such file or directory
--> Cannot open /dev/modem: No such file or directory
--> Cannot open /dev/modem: No such file or directory
/ #
If i give wvdialconf on terminal i am getting below msg.
/ # wvdialconf
Editing `/etc/wvdial.conf'.
Scanning your serial ports for a modem.
failed with 9600 baud, next try: 115200 baud
ttyS0<*1>: ATQ0 V1 E1 -- ttyS1<*1>: ATQ0 V1 E1 -- failed with 2400 baud, next td
ttyS1<*1>: ATQ0 V1 E1 -- failed with 9600 baud, next try: 115200 baud
ttyS1<*1>: ATQ0 V1 E1 -- and failed too at 115200, giving up.
ttyS2<*1>: ATQ0 V1 E1 -- failed with 2400 baud, next try: 9600 baud
ttyS2<*1>: ATQ0 V1 E1 -- failed with 9600 baud, next try: 115200 baud
ttyS2<*1>: ATQ0 V1 E1 -- and failed too at 115200, giving up.
Sorry, no modem was detected! Is it in use by another program?
Did you configure it properly with setserial?
Please read the FAQ at http://open.nit.ca/wiki/?WvDial
If you still have problems, send mail to <wvdial-list@lists.nit.ca>.
/ #
Pls help.
rgds,
raghava