Other Parts Discussed in Thread: UCD9244
I have two custom boards using the C6678. The only difference between the two boards is one has a Rev 1 C6678 and the other a Rev2. I use the UCD9244 with the 7242 for the CVDD power.
With the rev 1 silicon I do not ever see the VCNTL3 pin go low (I have a weak pull-ups on all the VCNTLs). With the Rev 2 silicon I do see the VCNTL3 pin toggle shortly after power-up. It's VID is 0x3F which is 1.103V.
The connection between the DSP and the UCD9244 passes through a level translator.
Why does the Smartreflex work for the Rev 2 but not the Rev 1 silicon? Could the Rev 1 be defective?