Hi,
Is it possible to set maximum and minimum i-frame interval for DM36x H264 codec?
Currently intraframeinterval = 30 and idrframeinterval = 30 settings are used.
But we need to set such that the i-frame occurs according to a set range. The range need to be set is 30 - 300. Which means after the IDR frame the next i-frame may occur after a minimum of 30 p-frames or a maximum of 300 p-frame.
Can this be set for DM36x codec?
-Vinay Bhargav