Hi,
I want to connect HDMI Input with OMAP-4460. So I decide to use Analog device's HDMI Rx ADV7611. I connected its video out put to CAM2 port and McBSP2 port for audio data.
HDMI Rx has MCLK, SCLK, LR CLK and Data Out lines from audio port. OMAP-McBSP has available lines are Data receive(Dr), Combined serial clock (CLKx) and combined frame synchronization (Fsx) and ABE_Clock input.
I connected MCLK to ABE_Clock input, SCLK to CLKx , DO to DI and LRCLK to FSx. I have two queries with this connection.
1. Can I use ABE_McBSP to receive audio data ?
2. Is my above connection is correct with McBSP port ?
Thanks in advance. Your valuable answer will help me to freeze my design.
Best Regards,
Hitesh Gambhava