Hello,
I would like to understand how we can configure the frame rate of display (with Links API) ? I tried to find in the code, but didn't.
I actually refer to the following passage from HDVPSS USER'S GUIDE:
"As shown in the figure, display driver controls configuration of VCOMP, CIG, EDE (TI816X only), CPROC (TI816X only), CSC, COMP and all the VENCs. It also configures the muxes to enable/disable the different paths to a particular VENC. It provides APIs to the application to configure these paths and to set the different frame rates and resolutions in the VENC. The display controller will provide necessary information to the display driver about the resolution and frame rate that it has to operate. This is abstracted from the application."
Best Regards,
Ran